Code snippets

Code snippets are predefined blocks of code for inserting into a structured text program. After inserting a snippet, fill in the parameters.
FactoryTalk Design Workbench
supports the following predefined code snippets:
  • IF-THEN-ELSIF-ELSE-END_IF
  • CASE
  • FOR
  • WHILE
  • REPEAT
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal