HSC Interrupt parameters

The HSC interrupt parameters are used to configure the start and mask options.

Auto Start (HSC0.AS)

Auto Start (HSC0.AS)
Parameter
Data format
HSC modes
User program access
HSCO.AS
Bit
0...9
Read-only
Auto Start is configured with the programming device and stored as part of the user program. The auto start bit defines if the HSC interrupt function automatically starts whenever the controller enters any run or test mode.

Overflow Mask (HSC0.MV)

The MV (Overflow Mask) control bit is used to enable (allow) or disable (not allow) an overflow interrupt from occurring. If the bit is clear (0), and an Overflow Reached condition is detected by the HSC, the HSC user interrupt is not executed.
The MV bit is controlled by the user program and retains its value through a power cycle. The user program must set and clear the MV bit.
Overflow Mask (HSC0.MV)
Parameter
Data format
HSC modes
User program access
HSCO.MV
Bit
0...9
Read-only

Underflow Mask (HSC0.MN)

Underflow Mask (HSC0.MN)
Parameter
Data format
HSC modes
User program access
HSCO.MN
Bit
2...9
Read-only
The MN (Underflow Mask) control bit is used to enable (allow) or disable (not allow) an underflow interrupt from occurring. If the bit is clear (0), and an Underflow Reached condition is detected by the HSC, the HSC user interrupt is not executed.
The MN bit is controlled by the user program and retains its value through a power cycle. The user program must set and clear the MN bit.

High Preset Mask (HSC0.MH)

High Preset Mask (HSC0.MH)
Parameter
Data format
HSC modes
User program access
HSCO.MH
Bit
0...9
Read-only
The MH (High Preset Mask) control bit is used to enable (allow) or disable (not allow) a high preset interrupt from occurring. If this bit is clear (0), and a High Preset Reached condition is detected by the HSC, the HSC user interrupt is not executed.
The MH bit is controlled by the user program and retains its value through a power cycle. The user program must set and clear the MH bit.

Low Preset Mask (HSC0.ML)

Low Preset Mask (HSC0.ML)
Parameter
Data format
HSC modes
User program access
HSCO.ML
Bit
2...9
Read-only
The ML (Low Preset Mask) control bit is used to enable (allow) or disable (not allow) a low preset interrupt from occurring. If this bit is clear (0), and a Low Preset Reached condition is detected by the HSC, the HSC user interrupt is not executed.
The ML bit is controlled by the user program and retains its value through a power cycle. The user program must set and clear the ML bit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal