Add and configure a high-speed counter (HSC) user interrupt

Use the following steps to add and configure an HSC interrupt.
To add and configure an HSC user interrupt
  1. In
    Project Organizer
    , right-click
    Programs
    , and then select
    New interrupt
    .
  2. Configure the HSC interrupt.
    1. In
      Name
      , enter the HSC interrupt name.
    2. From the
      Type
      list, select
      High speed counter (HSC)
      .
    3. From the
      ID
      list, select the HSC ID.
  3. Select
    Create
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal