DOY (check year for real-time clock)
The DOY instruction turns on an output when the value of the real-time clock (RTC) is in the range of the Year Time setting.
Operation details:
- If RTC is not present, the output is always off.
- Configure the Time input parameters with valid ranges as specified in the DOYDATA Data Type. An invalid value faults the controller when TimeX. Enable is set to TRUE and an RTC is present and enabled.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.DOY

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | Instruction enable.
|
TimeA | Input | DOYDATA | Year Time Setting of Channel A. Use the DOYDATA data type to configure TimeA. |
TimeB | Input | DOYDATA | Year Time Setting of Channel B. Use the DOYDATA data type to configure TimeB. |
TimeC | Input | DOYDATA | Year Time Setting of Channel C. Use the DOYDATA data type to configure TimeC. |
TimeD | Input | DOYDATA | Year Time Setting of Channel D. Use the DOYDATA data type to configure TimeD. |
DOY | Output | BOOL | If TRUE, the value of the real-time clock is in the range of the Year Time setting of any one of the four channels. |
DOYDATA Data Type
The following table describes the DOYDATA data type.
Parameter | Data Type | Description |
|---|---|---|
Enable | BOOL |
|
YearlyCenturial | BOOL | Type of timer (0:Yearly timer; 1:Centurial timer). |
YearOn | UINT | Year On value (must be in set [2000...2098]). |
MonthOn | USINT | Month On value (must be in set [1...12]). |
DayOn | USINT | Day On value (must be in set [1...31], determined by "MonthOn" value). |
YearOff | UINT | Year Off value (must be in set [2000...2098]). |
MonthOff | USINT | Month Off value (must be in set [1...12]). |
DayOff | USINT | Day Off value (must be in set [1...31], determined by "MonthOff" value). |
DOY examples
DOY function block diagram example

DOY ladder diagram example

DOY structured text example

(* ST Equivalence: *) TESTOUTPUT := DOY(TIMEA1, TIMEB1, TIMEC1, TIMED1) ;
Provide Feedback