Date Time instructions

Use Date Time instructions to control operations based on time or configure the calendar and the clock.
Date Time instructions
Instruction
Description
Turn on an output if the value of the real-time clock is in the range of the Year Time setting.
Reads the real-time clock (RTC) module information.
Sets RTC data to the RTC module information.
Computes the time difference between TimeA and TimeB.
Turns on an output if the value of the real-time clock is in the range of the Time of Week setting.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal