GE (>=)
The GE instruction compares Integer, Real, Time, Date, and String input values to determine whether the first is greater than or equal to the second.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.GE

Parameter | Parameter Type | Data Type | Description | |
|---|---|---|---|---|
EN | Input | BOOL | Instruction enable.
Applies only to ladder diagram programs. | |
i1 | Input | SINT USINT BYTE INT UINT WORD DINT UDINT DWORD | LINT ULINT LWORD REAL LREAL TIME DATE STRING | All inputs must be the same data type. The Time input applies to the structured text, ladder diagram, and function block diagram languages. |
i2 | Input | SINT USINT BYTE INT UINT WORD DINT UDINT DWORD | LINT ULINT LWORD REAL LREAL TIME DATE STRING | |
o1 | Output | BOOL | TRUE if i1 >= i2. | |
GE examples
GE function block diagram example

GE function block diagram example

(* ST Equivalence: *) aresult := (10 >= 25); (* aresult is FALSE *) mresult := ('ab' >= 'ab'); (* mresult is TRUE *)
Provide Feedback