TOF (timer, off-delay)
The TOF instruction increases an internal timer up to a given value.
Operation details: If the EN parameter is used with this instruction block, the timer starts incrementing when EN is set to TRUE, and continues to increment even if EN is set to FALSE.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.TOF

Parameter | Parameter type | Data type | Description |
|---|---|---|---|
IN | Input | BOOL | Input control.
|
PT | Input | TIME | Maximum programmed time. See Time data type. |
Q | Output | BOOL |
|
ET | Output | TIME | Current elapsed time. Possible values range from 0ms through 1193h2m47s294ms. |
TOF examples
TOF timing diagram

TOF function block diagram example

TOF ladder diagram example

TOF structured text example

Results

Provide Feedback