Fetch data logs

Use refresh button on the
<controller-name>: Manage data logs
page to do the following actions:
  • Fetch data logs for a specified time range from the memory card.
  • Fetch data logs for a specified time range from the computer when the controller is offline.
TIP:
  • If you fetch data log files when the controller is in
    Run
    mode, performance might be affected and the operation might take longer.
  • The fetching behavior only applies to data log files. The Header file is regenerated based on the data set configuration.
Prerequisites
  • The controller is online.
To fetch data logs
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Data Log
    .
  3. On the
    Data Log
    configuration page, select
    Manage data logs
    .
  4. On the
    <controller-name>: Manage data logs
    page, select refresh button to fetch the data log.
  5. Choose the date range for exporting data logs from the controller.
  6. (optional) When data logs for a particular period exist in the current project, select:
    • No, skip
      to skip fetching data logs for the period and use the data logs in the current project.
    • Yes, overwrite
      to fetch the data logs to overwrite the existing data logs for the period in the memory card or in the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal