Manage data logs

Use the
<controller-name>: Manage data log
page to do the following actions:
  • Fetch data logs for a specified time range from the memory card when the memory card is detected.
  • Fetch data logs for a specified time range from the computer when the controller is offline.
  • Delete data logs for a specified time range from the memory card.
  • Export the data logs to an XLSX or ZIP file to your computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal