Add a MicroLogix mapping

Use the
MicroLogix Mapping
configuration page to add a MicroLogix address value to a variable in the
Micro870
L70E or
Micro850
L50E controller. MicroLogix mapping supports up to 1,000 variables.
TIP: The program name that is associated with the selected variable follows the variable name. For example, in
DINT1@Prog1
,
DINT1
is the variable name, and
Prog1
is the program name.
To add a MicroLogix mapping
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    MicroLogix Mapping
    .
  3. In the
    MicroLogix Mapping
    gird, select Browse button or double-click
    Select variable
    .
  4. In the variable selector, locate and select the variable, and then select
    Select
    .
  5. (optional) Select a
    MicroLogix File Type
    for the variable.
  6. (optional) Change the
    File Number
    .
  7. Verify that the
    MicroLogix File Type
    is correct.
    TIP:
    • If the data type of the added variable is INT, select a
      MicroLogix File Type
      for the variable.
    • To read multiple MicroLogix addresses or a single address from an array, you must set the
      Micro800
      variable as an array. For example, to read the MicroLogix addresses from N7:0 through N7:10 or a single address N7:10, you must ensure that the
      Micro800
      variable that is mapped to the data file 7 is an array of 0 to 10 or any other arrays whose length is 11.
To delete a MicroLogix mapping, in the
MicroLogix Mapping
grid, right-click the variable, and then select
Delete
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal