MicroLogix Mapping configuration page
MicroLogix mapping allows communication between the following controllers:
- AnMicro870L70E controller and aMicroLogixorCompactLogix®controller for version 22.00 and later controller projects
- AnMicro850L50E controller and aMicroLogixorCompactLogixcontroller for version 23.00 and later controller projects
MicroLogix mapping supports up to 1,000 variables.
Use the
MicroLogix Mapping
configuration page to do the following actions:- Associate aMicroLogixaddress value with a variable in anMicro870L70E orMicro850L50E controller.
- Delete aMicroLogixaddress association.
- ExportMicroLogixmappings.
- ImportMicroLogixmappings.
Setting | Description |
|---|---|
File Number | Shows the number that is generated and assigned to the added variable. MicroLogix mapping supports a maximum of 1,000 variables.The File Number is a read/write integer from 0 through 999. Duplicate file numbers are not supported. |
Variable Name | Specifies the variable name that is associated with the MicroLogix address. |
Data Type | Specifies the data types that are available for configuration, including:
MicroLogix mapping is available for arrays with a string size of 82, but is not available for sub-elements of an array. |
MicroLogix File Type | Specifies the MicroLogix file type to which the value of a variable is converted.
|
Provide Feedback