Assign an alias name to a variable

An alias is an optional parameter that defines an alternative name for a global or local variable. Alias names must be unique within or across the
Name
and
Alias
columns.
To assign an alias name to a variable
  1. Open the global or local variable grid.
  2. Double-click the
    Alias
    cell of the variable, and then enter the alias name.
  3. Select
    Enter
    .
    TIP: If an alias name duplicates with an alias name or variable name, Error icon appears in the row header and the cell that contains the alias name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal