Open the local variable grid

Local variables are the variables assigned to a specific program in the project and are available only to the program.
To open the local variable grid
  • In
    Project Organizer
    , go to
    Programs
    <program-name>
    , and then under
    <program-name>
    , double-click
    Local Variables
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal