Replace an expansion module

Use these steps to replace an expansion module with another one in a controller project.
Prerequisites
  • To replace a module using the
    Replace module
    menu, at least one module must be added to the controller.
  • To replace a module using the
    New module
    menu, at least two modules must be added to the controller, and the module you want to replace is not in the last slot.
To replace an expansion module
  • Do one of the following:
    • To replace an expansion module using the
      Replace module
      menu
      1. In
        Project Organizer
        , go to
        I/O Configurations
        Expansions
        .
      2. Expand
        Expansions
        , right-click the module you want to replace, and then select
        Replace module
        .
      3. In
        Add module
        , select the new module, and then select
        Add
        .
      4. In
        Devices definition
        , configure the settings as needed, and then select
        OK
        .
    • To replace an expansion module using the
      New module
      menu
      1. In
        Project Organizer
        , go to
        I/O Configurations
        Expansions
        .
      2. Expand
        Expansions
        , right-click the module you want to replace, and then select
        Delete
        .
      3. In
        Warning
        , select
        NO
        .
      4. Under
        Expansions
        , right-click
        Available
        , and then select
        New module
        .
      5. In
        Add module
        , select the new module, and then select
        Add
        .
      6. In
        Devices definition
        , configure the settings as needed, and then select
        OK
        .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal