Expansion module configuration page

After adding an expansion module to a controller, in
Project Organizer
, under
Expansion
, a
<expansion-module-catalog-number>
node is created.
To open the expansion module configuration page, go to
I/O Configurations
Expansion
, and then double-click the expansion module.
On the expansion module configuration page, from the left pane, select a node to open the corresponding page.
Configuration page for different expansion modules
Expansion Module
Pages Created
Analog
  • Overview
  • Variable
  • Channel
  • Configuration
Digital
  • Overview
  • Variable
  • Configuration
Specialty
Overview
  • Overview
    page displays the catalog number, revision, module type, slot number, and the
    Device definition
    button. Selecting
    Device definition
    open a page to configure the slot, revision, and controller fault behavior for the expansion module.
  • Variable
    page lists the added variables with the variable names and data types.
  • Channel
    pages display the channel configurations for the expansion module.
  • Configuration
    page displays the module configuration settings.
For more information, see the introduction to individual expansion modules.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal