Add an expansion module to a controller project
Expansion I/O modules extend the capabilities of
Micro850
L50E and Micro870
L70E controllers by optimizing the flexibility of the I/O count and
type.For
Micro850
L50E controllers:- Add no more than four expansion modules.
- To avoid program compiling problems, limit the total number of digital inputs and outputs to:
- 192 or less forMicro850L50E controllers with 48 digital I/O points.
- 132 or less for otherMicro850L50E controllers.
For
Micro870
L70E controllers:- Add no more than eight expansion modules and no more than one power supply expansion module.
- To avoid program compiling problems, limit the total number of digital inputs and outputs to 304 or less.
To add an expansion module to a controller project
- InProject Organizer, go to .
- Right-clickExpansion, and then selectNew module.
- InAdd module, select an expansion module, and then selectAdd.
- InDevices definition, select the slot, revision, and controller fault behavior as needed, and then selectOK.
Provide Feedback