Invite Members

  • If you are a Project Admin,
    FactoryTalk DataMosaix SaaS
    provides you with the ability to invite members to your organization. While sending an invite, you can assign roles to the members, so once the members accept the invitation, the assigned roles are automatically applied. These invites expire after three days.
  • You can also see the history of the invitations you have sent and their statuses.
  • You can resend or delete an invite.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal