Navigation

The home page of
FactoryTalk DataMosaix SaaS
features a left navigation menu with the following tabs:
  • Manage Access
  • Extractor Info
  • Applications
  • Modeling
On the left navigation menu, you can also find direct links to
Main DataMosaix
(Cognite Data Fusion) and
FactoryTalk Hub
.
Left Navigation Menu
FactoryTalk DataMosaix SaaS Tabs
Manage Access
Allows you to modify users' roles using the
Members
sub-tab. You can view, edit, and modify the default and custom
Capability Groups
and
Roles
associated with the organization. You can invite members to the organization, view the status of the invite, resend or delete an expired invite using the
Invited Members
sub-tab. Also, you can activate or deactivate a specific functionality in
FactoryTalk DataMosaix SaaS
using the
Features
sub-tab.
Extractor Info
Allows you to register extractors that helps to push data to
FactoryTalk DataMosaix SaaS
.
Applications
Allows you to register applications that helps to view data.
Modeling
Allows you to create assets and helps organize assets and their properties in a hierarchical structure.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal