FactoryTalk DataMosaix SaaS Home Page Header
The home page header has the following options:
- Management Console
- Select Project
- Notifications
- Help and Support
- Profile Settings
FactoryTalk DataMosaix SaaS Home Page Header

Menu | Description |
|---|---|
![]() | Click the FactoryTalk DataMosaix SaaS logo to navigate to the Home Page. Clicking the logo displays the Manage Member Access page. |
| You can select a project from the project drop-down list to perform the required operations as per your role. |
| You can view the notifications you receive in FactoryTalk DataMosaix SaaS . |
| Click the Help and Support icon to view the following information:
|
| Click the Profile settings icon to view the username, email address, change language and the Sign Out option. |
Provide Feedback