Delete Extractor

Perform the following steps to delete extractor:
  1. On the Management Console, select the
    Extractor Info
    tab.
    The Extractors list is displayed.
  2. In the
    Actions
    column, click the Delete icon next to the extractor that you want to delete.
    The
    Extractor Detail
    page is displayed.
    NOTE:
    Once you delete an extractor, the extractor can no longer be used for sending data to
    FactoryTalk DataMosaix SaaS
    . Deleting an extractor removes all the information including the client secret. Hence, before deleting an extractor, verify the information so that you delete the correct extractor.
  3. Click
    Delete Extractor
    to proceed deleting the extractor.
    The
    Confirm Deletion
    dialog box is displayed.
  4. Click
    Yes
    to delete the extractor.
    The extractor is removed from the Extractor List.
NOTE:
Perform the following steps to decommission a running
FactoryTalk Optix
extractor:
  1. Navigate to the
    FactoryTalk Optix Studio
    .
  2. Stop the running project.
  3. Uninstall the
    FactoryTalk Optix
    connector or remove the custom data source from the
    FactoryTalk Optix
    project.
  4. Navigate to the
    FactoryTalk DataMosaix SaaS
    .
  5. Delete the extractor you want to decommission. For more information, refer to Delete Extractor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal