WAN/Wireless Communications
Communications across anything slower than a 100mpbs, wired LAN can present negative impact on overall system performance. Aside from the question of network security, which is outside the scope of the document, two key factors are the speed and stability of the network. To mitigate problems due to signal interference or timeouts, it is strongly recommended to use Remote Desktop Services to bridge any WAN/Wireless communications. See the “Remote Desktop Services” section of this document for more information on implementing Remote Desktop Services.
Provide Feedback