FactoryTalk AssetCentre Web Client
The FactoryTalk AssetCentre Web client requires no installation, instead accessing the server through an internet browser. The web client can be run on a computer. The web client can be accessed at http://<FQDN>/RockwellSoftware/AssetCentreWebClient.
The web client can be used to view information about the FactoryTalk AssetCentre system. In Design mode, you can also operate in web client, such as check in and check out files.
Client performance is based on the number of web clients simultaneously requesting information from the server, and the size of the AssetCentre system. As the number of assets, schedules, etc grow, additional time will be required to process each client request.
TIP:
FQDN
is the fully qualified domain name of the FactoryTalk AssetCentre Server computer.If you are changed the default port in site binding, you need to include the self-defined port number in the computer name part in the form as
MYSERVER:PortNumber
.Provide Feedback