Configure Idle Time-out property in Internet Information Services (IIS) Manager

When no interaction with the web client has occurred for 20 minutes, you will be automatically signed out. You can adjust the Idle Time-out property using the Internet Information Services (IIS) Manager.
To configure Idle Time-out property in Internet Information Services (IIS) Manager
  1. Open
    Internet Information Services (IIS) Manager
    on the FactoryTalk AssetCentre server computer.
  2. In the
    Connections
    pane, select
    Application Pools
    .
  3. Under Application Pools, right-click
    AssetCentreWebClient
    , and then select
    Advanced Settings
    .
  4. Do the following to configure Idle Time-out property:
    • To adjust the length of time before the user is automatically signed out:
      Adjust
      Idle Time-out (minutes)
      as desired. The default length of time is 20 minutes.
    • To prevent the user from being automatically signed out:
      Change
      Idle Time-out Action
      by selecting
      Suspend
      from the dropdown menu. The default selection is Terminate.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal