Renaming the AssetCentre Database
While it is possible to rename the FactoryTalk AssetCentre database from the default "AssetCentre", it is not recommended. In particular, all upgrade scripts are hard-coded to look for the "AssetCentre" database, meaning that if it has been renamed, it must be named back to the default prior to any upgrades taking place.
Provide Feedback