Impacts on FactoryTalk AssetCentre functions if an activation expires
If an activation expires, certain FactoryTalk AssetCentre functions are affected. When FactoryTalk AssetCentre server activation expires, you cannot:
- Enter design mode
- View logsIf server activation expires, FactoryTalk AssetCentre records log entries but you cannot view them.
- Perform achieve operations except for getting a file or binder.
When a Disaster Recovery activation of a scheduled asset type expires, the following operations are not supported:
- Create a schedule
- Run a schedule manually
- Run a schedule automatically at its next scheduled time
- Modify timing properties of a schedule
Provide Feedback