Tools menu

The following table shows the commands on the
Tools
menu.
Command
Description
Options
Shows the
Options
dialog box in which you can specify some overall settings regarding the display and action of the FactoryTalk AssetCentre desktop client on this computer. For example, set the refresh rate for the Logs tab or specify a software program that the Archive component should use to open files with a certain extension.
Archive Cleanup Wizard
Opens the Archive Cleanup Wizard that allows you to remove old versions of files from Archive to free up disk space.
Log Cleanup Wizard
Starts the Log Cleanup Wizard which you can use to decrease the size of the database.
Management of Change Admin
Opens the Management of Change Admin website which you can use to configure the Management of Change settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal