Help menu
The following table shows the commands on the
Help
menu.Command | Description |
|---|---|
Contents | Shows the online help showing the Welcome page. Use the Contents or Search tab to find the information you need. |
Show Help | Shows the online help related to the part of the software you are currently using. |
Installation Guide | Shows the FactoryTalk AssetCentre Installation Guide in Adobe PDF format. |
Quick Start | Show the first page of the Quick Start series in the online help. The Quick Start provides instructions for initial setup and beginning use of the FactoryTalk AssetCentre software. |
About | Shows the About box which contains information about the version of FactoryTalk AssetCentre and Rockwell Automation contact information. |
Provide Feedback