Setting up and editing schedules
This topic lists some issues when setting up and editing schedules.
Message: Unable to create a new schedule ... No licensed agents are available ...
This means that the capability for the selected device type is not activated.
For this type of device ... | You need this type of activation … |
|---|---|
Rockwell Automation devices such as Allen-Bradley PLC-5 controllers and PanelView interfaces | Disaster Recovery for Rockwell Automation |
FANUC robots | Disaster Recovery for FANUC |
Motoman robots | Disaster Recovery for Motoman |
ABB robots | Disaster Recovery for ABB |
Generic FTP | Disaster Recovery for FTP |
Siemens S7 Controllers (STEP7) | Disaster Recovery for Siemens S7 |
Siemens S7 Controllers (TIA Portal) | Disaster Recovery for Siemens S7 TIA Portal |
Mitsubishi Controllers (GX Works2) | Disaster Recovery for Mitsubishi GX Works |
Mitsubishi Controllers (GX Works3) | Disaster Recovery for Mitsubishi GX Works |
Schneider Controllers (Control Expert) | Disaster Recovery for Schneider Control Expert |
Custom Device | Disaster Recovery for Custom Device |
Remote Computers | Disaster Recovery for Remote Computer |
Asset Inventory | Disaster Recovery for Asset Inventory |
Message: Failed to create RSLogix 5 [or 500] data [or program ladder] file list
This message appears if you do not have the RSLogix 5 or RSLogix 500 programming software installed on the client computer on which you are specifying which files and data will be compared during a Backup and Compare operation. Install the RSLogix programming software on the client computer or use a client computer that has the programming software.
Some Allen-Bradley Logix 5000 controller assets are not shown when setting up a Change Detect schedule.
If Change Detect Capable is blank or false on the controller asset's
Properties
dialog box, then the controller is not shown on page 3 of the New Schedule Wizard and cannot be added to the schedule.Provide Feedback