Define date and time for a fuzzy search of logs
Use the
New Condition
or Condition Properties
dialog box to define date and time for a fuzzy search on the logs generated based on date and time. This function applies to Date
, Activity Date/Time
, Occurred Time
, and Logged Time
columns.To define date and time for a fuzzy search of logs
- In theNew ConditionorCondition Propertiesdialog box, select a column associated with date and time such asOccurred TimeorLogged Time.
- (optional) Clear theIgnore timecheck box to set time.It is selected by default to disable the time setting.
- SelectAbsolute date/timeorRelative to date/time report is run.
- Absolute Date/TimeEnter or select the date and time so that the search will return activities that occurred at the specified time according to the server computer’s time settings.You can use this option to search an activity that you know occurred on the exact day.
- Relative to date/time report is runEnter or select the date and time so that the search will return activities that occurred at the specified time according to the client computer’s time settings.You can use this option to search an activity that you know occurred within the last week but you do not know the exact day.For Example, the client computer's date is December 3, 2020. If you select this date/time type and specifyDate/Time selection optionsas two days ago, the relative date will be defined as December 1, 2020 and then the search will be run based on this date.
- Select date/time options.
- Equal ToEnter or select the date and time (or days and hours ago) for which you want to search.For Example, the the computer's date is December 3, 2020. If you selectRelative to date/time report is runand specify two days ago for this option, the search will return activities occurred on December 1, 2020.
- BetweenEnter or select the start and end time for which you want to search. Between specifies a period including the start and end time.For example, the the computer's date is December 3, 2020. If you selectRelative to date/time report is runand specify two days ago in the upper date box and one day ago in the lower date box, the search will be run to return activities occurred between December 1, 2020 and December 2, 2020.
- BeforeEnter or select the date prior to which the activities happened. The search will return activities that occurred prior to the specified time, not including activities that occurred at the specified time.For example, the client computer's date is December 3, 2020. If you selectRelative to date/time report is runand specify two days ago for this option, the search will return activities that occurred prior to December 1, 2020, not including activities that occurred on December 1, 2020. Thus, to include activities that occurred on December 1, 2020, specify one day ago for this option, or use theEqual Tooption to specify that exact date.
- AfterEnter or select the date later than which the activities happened. The search will return activities that occurred later than the specified time, not including activities that occurred at the specified time.For example, the client computer's date is December 3, 2020. If you selectRelative to date/time report is runand specify two days ago for this option, the search will return activities that occurred later than December 1, 2020, not including activities that occurred on December 1, 2020. Thus, to include activities that occurred on December 1, 2020, specify three days ago for this option, or use theEqual Tooption to specify that exact date.
- SelectOK.
Provide Feedback