Condition - Source

How do I open the New Condition dialog box?
  1. Select
    View > Searches
    , or click the
    Searches
    button.
  2. Select the search to contain the new condition.
  3. Click the
    Conditions
    tab.
  4. Click the
    New Condition
    button.
How do I open the Condition Properties dialog box?
  1. Select
    View > Searches
    , or click the
    Searches
    button.
  2. Select the search containing the condition to modify.
  3. Click the
    Conditions
    tab and select the desired condition.
  4. Click SearchesProperties.
Use the
New Condition
dialog box or
Condition Properties
dialog box to specify or modify the content for which you would like to search. For example, create or modify a condition that searches for log records generated by a specific source, for example, the software product Logix Designer.
TIP:
Resource, while sometimes the name of the hardware object to which the action happened, can also be a software product. Therefore, the source and resource can be the same software product that logs an entry. The
Source
column of data appears in the Event Log, the Audit Log, and the Diagnostics and Health Log.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal