Column headings on the page
These values are all supplied by the block properties in the S7 project.
- BlockThe name of the block, for example, DB4.
- Symbolic NameSymbolic information is stored in Configuration Data, not Backup Data. When possible, the software shows the symbolic name for the block stored in Configuration Data.
- Symbolic CommentSymbolic information is stored in Configuration Data, not Backup Data. When possible, the software shows the symbolic comment for the block stored in Configuration Data.
- Interface TimestampThe date the interface was last modified.
- Code TimestampThe date the code was last modified.
- VersionThe version number of the block in the S7 project.
Provide Feedback