E - L

- E -
Event Log
The Event Log shows database information regarding events that occur in the system. Events are generally system initiated. For example, an upload occurred as scheduled, or an alarm condition occurred. Only events that occur in FactoryTalk enabled products are recorded in the Event Log.
- F -
FactoryTalk Activation Manager
The FactoryTalk Activation Manager is a software program that manages activations for the Rockwell Software products installed on the computer.
Run the FactoryTalk Activation Manager from the
Windows Start
menu:
Start > Rockwell Software > FactoryTalk Activation Manager
.
(If you are using FactoryTalk Activation version CPR 9 SR 2 or earlier, this software was called the FactoryTalk Activation Tool.)
FactoryTalk Administration Console
Part of the FactoryTalk Services Platform, FactoryTalk Administration Console is an optional, stand-alone tool that allows configuring, managing, and securing applications.
To run the FactoryTalk Administration Console from the
Windows Start
menu, select
Start > Rockwell Software > FactoryTalk Administration Console
.
FactoryTalk Help
The
FactoryTalk Help
contains information on several FactoryTalk components including the FactoryTalk Administration Console, FactoryTalk Directory, and FactoryTalk Security. To access the
FactoryTalk Help
, select
Start > Rockwell Software > FactoryTalk Help
.
FactoryTalk Security
Formerly known as RSAssetSecurity.
A set of security services integrated into the FactoryTalk Directory. Use FactoryTalk Administration Console or FactoryTalk View Studio to configure these security services.
FDT
Field Device Technology standardizes the communication interface between field devices and systems. FactoryTalk AssetCentre uses FDT to access and configure physical devices through any protocol. See the FDT Group website for more information: www.fdtgroup.org.
Final command line
The final command line for custom devices is used to run the backup, compare, or post-backup operations for custom devices in Windows Command Prompt. It is editable in the
Command
field in the
Options
dialog box
: Custom Devices.
The final command line is composed of two parts, Program and Arguments.
- G -
Get
Retrieve a read-only copy of a file to your current working folder. FactoryTalk AssetCentre's Archive is like a library, therefore getting a file is like photocopying a document and leaving the original in the library. Generally, you get a file when you only want to view the file, and do not want to edit it. However, you have the option of retrieving a writable copy of a file when you get it.
- K -
Key file
A key file for a binder is the file that will be opened when the binder is opened through FactoryTalk AssetCentre (or through a desktop shortcut created from within FactoryTalk AssetCentre). A file association for that type of file should be set in
Tools > Options
to specify what software to use to open the file. For example, if the binder contains an RSView project, specify the .RSV file as the key file because that is the file that will open the project in RSView. In
Tools > Options
specify RSView as the software to use to open .rsv files.
- L -
links
Links connect steps to transitions and transitions to steps. The direction of the link is always from the bottom of one element to the top of another element. Links have no runtime function other than defining the order of sequence elements.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal