Specify addressing information for Allen-Bradley MicroLogix controller
You must be connected to the control network to specify addressing information for the device.
To specify the addressing information
- Click anywhere in theAddressing Infofield and then click
. Use the Selecting Device for Asset Typedialog box to browse the network for the Allen-Bradley MicroLogix controller that you want to add. When you have found the desired controller, select it and clickSelect. - Complete the remaining fields.
Provide Feedback