Authentication dialog box
How do I open the Authentication dialog box?
You can open the
Authentication
dialog box while adding an Allen-Bradley E300 Overload Relay asset to the asset tree or while editing the asset's properties.While adding an asset to the asset tree:
- If you are not in Design mode, click
. - Drag an asset from the Asset Catalog to add it to the Asset View.
- Click anywhere within theAuthenticationfield, and then click
.
While editing an asset's properties:
- If you are not in Design mode, click
. - Double-click an asset in the asset tree.
- Click anywhere within theAuthenticationfield, and then click
.
Use the
Authentication
dialog box to supply user credentials for the physical device that you want to connect to and add as an asset.The following table lists the properties in the dialog box.
Properties | Descriptions |
|---|---|
User name | Enter the user name to log on to the Allen-Bradley E300 Overload Relay. |
Password | Enter the password of the user name. |
Test Connection | Click this button to validate whether the credentials are all correct.
Tip : In certain cases, after clicking Test Connection , the Authentication dialog box stops responding before showing the connection failed message. You need to wait for several seconds for the system to be responsive. |
OK | Click to confirm all the information entered in this dialog box. It is only available when all the information is valid after clicking the Test Connection button. |
Cancel | Click to close this dialog box. No changes made will be saved. |
Help | Click to open Help. |
Provide Feedback