Specify addressing information for Allen-Bradley PanelView Plus operator interface

You must be connected to the control network to specify addressing information for the device.
To specify the addressing information
  1. Click anywhere in the
    Addressing Info
    field and then click browse_button_small. Use the
    Selecting Device for Asset Type
    dialog box to browse the network for the Allen-Bradley PanelView Plus operator interface that you want to add. When you have found the desired device, select it and click
    Select
    .
  2. Complete the remaining fields.
    TIP:
    You must have the RSLinx Enterprise or
    FactoryTalk Linx
    software installed on the FactoryTalk AssetCentre client computer to configure these settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal