Unblock a Management of Change workflow
When the Management of Change workflow starts to check in or check out files and binders associated with the selected asset, you can reset the Management of Change workflow status of files and binders in Initiated Check-in Workflow, Completed Check-in Workflow, Initiated Check-out Workflow, and Completed Check-out Workflow statuses.
Prerequisites
- To unblock a workflow, you must have theUnblock MoC workflowpermission.
To unblock a Management of Change workflow
- SelectView > Archive, or click theArchivebutton.
- In the asset tree, select the files and binders associated with selected assets which are in the Management of Change workflow.
- Select theUnblock Workflowbutton.
- In theUnblock Workflowdialog box, enter the comments.
- SelectOK.
Provide Feedback