Export the Asset Inventory scanning result

You can export the Asset Inventory scanning result to an .XML file for further analysis.
To export the Asset Inventory scanning result
  1. In the
    Asset Inventory
    window, click Asset Inventory export.
  2. Use the
    Save As
    dialog box to provide a file name and location for the exported file.
  3. Click
    Save
    . The Asset Inventory scanning result is saved in .XML format.
    TIP:
    If any changes made to additional information are not checked in before exporting, the changes cannot be exported.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal