FactoryTalk AssetCentre Import Export Utility
The
FactoryTalk® AssetCentre
Import Export Utility allows you to create a mass of
new assets, import assets with customized properties, and edit or duplicate assets of an
asset node.
IMPORTANT:
- This tool does not support exporting a CSV file from one FactoryTalk AssetCentre system and importing it into another FactoryTalk AssetCentre system.
- This tool does not support operations forSiemens®S7 Controller (TIA Portal™), Mitsubishi® Controller (GX Works2™), Mitsubishi Controller (GX Works3™), and Schneider® Controller (Control Expert) asset types.
- The version of this tool must match the version of the FactoryTalk AssetCentre system. For example, the FactoryTalk AssetCentre Import Export Utility version 15.00.00 should not be used with FactoryTalk AssetCentre version 16.00.00. Starting from FactoryTalk AssetCentre version 16.00.00, you can install this tool by selecting theAssetCentre Import Export Utilityoption during the FactoryTalk AssetCentre Desktop Client or FactoryTalk AssetCentre Custom installation. This option is selected by default. For more information, see Install the FactoryTalk AssetCentre Desktop Client software in theFactoryTalk AssetCentre Installation Guide.
This tool provides the following four options:
- New mass creationCreates a group of new assets of different types in the asset tree all at once.
- New importImports a batch of assets with user-defined asset properties.
- Edit assets of an asset nodeEdits properties of assets under a certain asset node.
- Duplicate assets of an asset nodeDuplicates an existing node of assets in the asset tree.
To create, import, edit, or duplicate assets, make sure that no other user in the system is
in Design mode in FactoryTalk AssetCentre desktop client. This allows the tool to update the
asset tree as designed.
Provide Feedback