Configure automatic database index maintenance
Automatic database index maintenance rebuilds the fragmented indexes regularly if the index fragmentation rate exceeds the configured threshold. If the fragmentation rate doesn't exceed the threshold, an email will be sent notifying the database status.
Prerequisites
- Make sure you have theConfigure Database Maintenancepermission.
To configure automatic database index maintenance
- OnTools, selectDatabase Management.
- OnDatabase Management, selectDatabase Maintenance.
- Select theSchedule automatic database index maintenancecheckbox.
- In the percentage list, select a value or enter any integer from 20 through 50.
- In theStart onlist, select a date, and enter a time when the automatic database maintenance starts. Make sure that the time format follows hh:mm AM or PM.TIP:
- The index rebuild process may take several minutes to complete and may impact the system performance. Set the maintenance time during a server null time when no scheduled tasks or user interaction is taking place if possible.
- When updating from FactoryTalk AssetCentre version 10.00.00 to version 11.00.00, it is recommended to customize the date and time settings. If not, the automatic database maintenance will follow the previous configuration in version 10.00.00.
- In theweek(s)box, select the up and down arrow or enter an integer as the frequency for automatic database maintenance.
- Next to theEmail notificationbox, select the browse button, and then choose the email recipients to receive the database maintenance status. SelectSubmit.
- SelectSave.
Provide Feedback