About Database Information
The following table shows the categories of
Database Information
and their meanings.Item | Description |
|---|---|
Database Name | Shows the name of the database. |
Database Version | Shows the database's version information. |
Total database / allocated size | Shows the database's size. |
Unallocated Size | Shows the database's unallocated size. |
Used by Archive | Shows the space that is used by file images and the size of the activity log. |
Used by Log | Shows the size of the event log, audit log, and diagnostics and health log. |
Provide Feedback