Column headings on Searches

The following table shows the column headings on
Searches
and their meanings.
Column Headings
Description
Active
Indicates whether the scheduled search is active. The active scheduled search will run at the scheduled time.
Status
Shows the scheduled search status: Waiting To Run, Running, Stopping, and Disabled.
Name
Shows the search name that must be unique.
Description
Shows the description of the search definition. This column is not shown by default. To show this column, hover over any column heading, select ftac_web_archive filter1, and then select ftac_web_archive filter3 to configure the columns to show.
Last Time
Shows the last time the scheduled search ran. If the scheduled search has not run previously, the box is empty.
Next Time
Shows the next time that a scheduled search will run. If the scheduled search is inactive, this box is empty.
Completion Email List
Shows the recipients who will receive notifications when the search completes.
Timing Properties
Shows the schedule to run the search. It shows the frequency and maximum runtime.
Action
Starts or stops the search.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal