About running a schedule
You can run schedules automatically or manually. Running a schedule manually will send emails to your distribution list instead of having to wait for the operation's next run time. Running a schedule manually does not affect that schedule's next run time.
Once you run a schedule manually, it returns to Waiting to Run status. If running the schedule manually causes the schedule to run through its start time, FactoryTalk AssetCentre Web Client does not attempt to run the previously scheduled operation, the message "The schedule has tripped but didn't run because it is running" is logged to the AssetCentre Event Log, and the schedule waits to run again at its next start time.
Provide Feedback