Run a schedule manually

Run a schedule manually without waiting for its next scheduled run time. You cannot manually run a schedule that has a Running status. Running a schedule manually will send emails to your distribution list instead of having to wait for the operation's next run time. Running a schedule manually does not affect that schedule's next run time.
Once you run a schedule manually, it returns to Waiting to Run status. If running the schedule manually causes the schedule to run through its start time, FactoryTalk AssetCentre web client does not attempt to run the previously scheduled operation, the message "The schedule has tripped but didn't run because it is running" is logged to the AssetCentre Event Log, and the schedule waits to run again at its next start time.
Prerequisites
  • To run schedules, you must have the
    Command a schedule
    permission.
  • To activate schedules, you must have the
    Edit a schedule
    and
    Command a schedule
    permission.
To run a schedule
  1. On
    Schedules
    , select a schedule that you want to run.
  2. In the
    Action
    column, select ftac_web_schedules_start.
    TIP:
    When you start an active schedule, ftac_web_schedules_running indicates that you cannot stop it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal