View dashboard
FactoryTalk AssetCentre web client provides a Lifecyle Information dashboard with widgets that can be used to monitor and analyze lifecycle information.
To view dashboard
- OnLifecycle Information, select the RAAI file in the asset tree view.TIP:Select the parent node will include all the RAAI files in the parent container.
- Select the dropdown arrow next toSelect version.
- Filter the devices byFilter by versionorFilter by label, select a RAAI file version, and then selectOK.
- SelectUpdate lifecycle information.
- SelectDashboard, and then the lifecycle information shows.
Provide Feedback