Configure security
By default, all users and the Administrators group in
FactoryTalk® Directory
can perform any task in the FactoryTalk AssetCentre software. To deny specific users the right to perform tasks in FactoryTalk AssetCentre Web Client, you must edit the Feature Security settings in the FactoryTalk Administration Console.
IMPORTANT:
Never explicitly deny rights to the All Users or Administrators group in FactoryTalk. Rather, set up specific user groups of your own and deny rights to those groups. Denying rights to All Users or Administrators could lock everyone out of the system and would deny rights in all FactoryTalk-enabled products.
To configure security settings
- From the Start menu, selectRockwell Software>FactoryTalk Administration Console.
- Sign in to the Network directory using a FactoryTalk administrator account.
- In theExplorerpane of the FactoryTalk Administration Console, navigate toSystem>Policies>Product Policies>FactoryTalk AssetCentre.
- Double-clickFeature Security.IMPORTANT:Here is also a Server Settings object in the FactoryTalk AssetCentre folder. Do not attempt to change any of the settings in this object. Doing so may render your FactoryTalk AssetCentre system inoperative. If you need to change server settings (to use a different mail server, for example), from WindowsStartmenu, selectRockwell Software>FactoryTalk AssetCentre Server Settings.
- In theFeature Security Propertieswindow, select the policy that you want to change, and then select the browse button for the policy.
- In theConfigure Securable Actiondialog, select the user or group for whom you want to assign permissions. If the user or group does not appear in the list, clickAdd, clickShow all, select the user or group, and then clickOK.
- Select the appropriate box to allow or deny the user permission to the selected feature.
- SelectOK.
Provide Feedback