Items in the Undo Check Out dialog

The following table shows the items in the
Undo Check Out
dialog and their meanings.
Items
Descriptions
Recursively undo a check out from subfolders
Select this option to undo the check-out operation of all items within the asset's subfolders.
This option is only available when you select an asset that contains subfolders or other assets in the asset tree.
Comments
Enter an optional comment to track work. The maximum length of a comment is 2,500 characters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal