Items in the container or asset pane
The information in the following table shows when a container or an asset is selected in the asset tree.
Column Headings | Descriptions |
|---|---|
Name | The name of a file contained in the asset. If the file is pinned or checked out,
a pushpin icon or check mark appears next to the file. |
User | The signed-in user who checked out the file. It is empty if the file is checked
in. |
Check Out Location | The location where the file is checked out. The default path is
C:\Users\Signed-in User\Downloads. |
Provide Feedback