Check Out dialog

How do I open the Check Out dialog?
  1. On
    Assets
    , expand the asset tree, and then select a file, a binder, or an asset containing the files that you want to check out.
  2. Select the
    Check Out
    button.
Use the
Check Out
dialog to retrieve a copy of a binder or file to C:\Users\Signed-in User\Downloads on your computer so that you can edit the file or binder. Only one user can check out and edit a file or binder at a time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal