Items in the Check In dialog
The following table shows the items in the
Check In
dialog and their meanings.Items | Descriptions |
|---|---|
Recursively check in files from subfolders | Select this option to check in all files or binders within the asset's
subfolders. This option is only available if you select a folder, an asset, or a container in
the asset tree. |
Comments | Enter an optional comment to track work. The maximum length of a comment is 2500
characters. Note: The value assigned to the Allow Empty Comment at Check In
security setting decides whether you must enter a comment. |
Provide Feedback