Check In dialog
- OnAssets, expand the asset tree, and then select a file, a binder, or an asset containing the files to check in.
- Select theCheck Inbutton.
Use the
Check In
dialog to return a file or binder on your computer to the archive
database. Checking in a file or binder makes a new version in which changes are backed up
and protected.Provide Feedback